Hello
I used the safe library in my program.Need to pass SL4 safety certification.
Now the Third-party certification company ask me .How to follow the rules of API functions.
for example SL_SelfTest_Flash
Note : Refer to Safety Manual for TMS570LS31x/21x and RM48x Hercules ARM Safety Critical Microcontrollers (section on Primary Embedded Flash and RM48x/TMS570LS31x 16/32-Bit RISC Flash Microcontroller TRM (section F021 Flash Module Controller)
Note: For FLASH_ECC_TEST_MODE_2BIT_FAULT_INJECT the fault is injected in the subsequent read of the corrupted flash area by the application. The application must take care to restore the flash diagnostic control registers . Note: FLASH_HARD_ERROR_LIVELOCK is not supported in this release.
Note : Any ESM errors that activates nError Pin while running this Test are unconditionally reset.
TRM paper Did not see special content