Hello,
I have installed the browser extension and local application to connect to the board with CCS Cloud, but am unable to program the board.
I can connect no problem:
But cannot run:
This is how the board is recognized on dev.ti.com's home page:
In device manger, I see:
- Under "Ports": "Stellaris Virtual Serial Port"
- Under "Other devices": two instances of "In-Circuit Debug Interface"
Also, in ticloudagent_install.log I see the lines:
[13:21:24] PNPUTIL: Drivers installed successfully. Installing target support (This may take some time) Executing TICloudAgent/node.bat Script exit code: 1 Script output: Script stderr: Operation failed: no valid command line parameter passed Error running TICloudAgent/node.bat : Operation failed: no valid command line parameter passed