This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C123GXL: Errors when using cloud tools (CCS Cloud, UniFlash, etc.)

Part Number: EK-TM4C123GXL

Hello,

I have installed the browser extension and local application to connect to the board with CCS Cloud, but am unable to program the board.

I can connect no problem:

But cannot run:

This is how the board is recognized on dev.ti.com's home page:

In device manger, I see:

  - Under "Ports": "Stellaris Virtual Serial Port"

  - Under "Other devices": two instances of "In-Circuit Debug Interface"

Also, in ticloudagent_install.log I see the lines:

[13:21:24] PNPUTIL: Drivers installed successfully.
Installing target support (This may take some time)
Executing TICloudAgent/node.bat 
Script exit code: 1

Script output:
 

Script stderr:
 Operation failed: no valid command line parameter passed


Error running TICloudAgent/node.bat : Operation failed: no valid command line parameter passed