Other Parts Discussed in Thread: HALCOGEN
The code solution for the issue SSWF021#45 in errata SPNZ226A can be generated in HaldCoGen tool.
We are not using the DCC module, so the issue DCC#24 is not affecting us.
Question: Does the code fof HaldCoGen tool for resolving SSWF021#45 consider the issue DCC#24?
Note: The code of HalCoGen is the same spna233b has. The function that use the DCC is called check_frequency(uint32 cntl_clksrc).
the previous function uses Single Shot mode.