This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/BOOSTXL-SENSHUB: PROBLEM WHILE OBSERVING THE PRESSURE SENSOR OUTPUT

Prodigy 50 points

Replies: 2

Views: 543

Part Number: BOOSTXL-SENSHUB

Tool/software: Code Composer Studio

Hello all,

I am trying to interface Senshub with TIVA TM4C123GH6PM for measurement of pressure.

I have interfaced the two modules as per the guidelines given.

Also,I have taken the example code for pressure sensor from the libraries.

But,I am facing an issue of how to see the output of the pressure sensor on the CCS.

I want to measure air pressure with the sensor.

Also,can I observe the output on energia?

Please suggest  me appropriate solution for the same.

Thanks in advance.

2 Replies

  • May we note that your post's Subject lists, "Problem while observing" (sensor output) yet your (post) notes, "How to see the output?"

    That's somewhat confused and/or in conflict - is it not?

    Further - even multiple readings of all "Senshub" literature will aid - is that not so?
  • Did you import this example: "C:\ti\TivaWare_C_Series-2.1.4.178\examples\boards\ek-tm4c123gxl-boostxl-senshub\pressure_bmp180"? If so, here are the instructions from the readme.txt file:

    Connect a serial terminal program to the LaunchPad's ICDI virtual serial
    port at 115,200 baud. Use eight bits per byte, no parity and one stop bit.
    The raw sensor measurements are printed to the terminal. The RGB LED
    blinks at 1Hz once the initialization is complete and the example is
    running.

    Best Regards,
    Bob Crosby

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.