This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

RTOS/TI-RTOS-MCU: Where is the latest TI-RTOS configuration tool for CC32xx

Prodigy 80 points

Replies: 6

Views: 156

Part Number: TI-RTOS-MCU

Tool/software: TI-RTOS

I'm in the process of taking the TI-RTOS training, and was wondering where the GUI configuration tool resides for CCS V8?  I have downloaded a xdctool zip file for V8, but how do you plug it into CCS?

  • Hi,

    You need to right click on the .cfg file and edit it with XGCONF.

    Todd
  • In reply to ToddMullanix:

    Thank you.  I'm now able to see the XGCONF tool.

    However, I have a more questions:

    1) I imported the SWI example from the CC3220SF repository, and viewed the swi.cfg settings in XGCONF.  The SWI example uses both HWI and SWI, but they are not shown in the "instance" tab.  Is there a way to have them show up?  Maybe an import or sync option?

    2) If you are starting a TI-RTOS project from scratch, then how do you start XGCONF?  It seems like the only way right now is to right click on an existing .cfg file.

  • In reply to Rick Policy:

    Hi Rick,

    Which version of CCS are you using? We've had some problems with some of the 8.0 or 8.1 versions in reagrds to the XGCONF display. Can you attach a snapshot of the GUI 's instance window that you mentioned and also the text that creates the Hwi and Swi instances from the .cfg file.

    We used to default to XGCONF, but more customers use the text approach. Internally we use it more also and prefer it when communicating among ourselves and with customers. It's easier to give a couple lines of text instead of a snapshot.

    Todd
  • In reply to Rick Policy:

    I'm using CCS Version 8.3.

    Attached are code, cfg, and XGCONF snippets...

    XGCONF Issue.pdf

    Code snippet:
    Snapshot from XGCONF:
     
    Swi.cfg snippet:
     

  • In reply to Rick Policy:

    Thanks.

    You are creating the Swi dynamically (during runtime). This will not show up in XGCONF. XGCONF allows you to create objects "statically". Hopefully this page will make this more clear: processors.wiki.ti.com/.../TI-RTOS_Object_Creation_Comparison

    Todd
  • In reply to ToddMullanix:

    Thanks again Todd, this resolves my issue.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.