Hi,
I am working on a design that uses the Tiva TM4C1237E6PM device. I am running very low on GPIO pins and would like to reclaim unused ADC inputs. I used the pin mux tool to assign my I/O, and when I enable ADC0, 12 AIN pins turn green. I only need 4 channels of ADC, so I would like to re-assign some of these unused ADC channels to GPIO. Using the tool I select an AIN pin and reassign to GPIO input, and it turns red, indicating a collision.
Does this mean that I cannot reclaim these pins as GPIO? Can I reconfigure these pins after start up to GPIO, either input or output? Do I need to terminate any unused AIN inputs?
I have the same question regarding USB0, I intend to only function as a USB host, and would like to reclaim PB0 and PB1. The datasheet implies that this can be done, but I want to make sure before finalizing my pin assignments.
Thanks,
ART