I'm designing schematics for TM4C129ENCPDT with Ethernet.
I need an ESD protection.
I found some design notes:
In TM4C129X System Design Guidelines SLVU2.8-4 has using with ESD level of 2.8 V.
In TIDA-00226 TPD4E1U06 has unsing with ESD level of 6.5 V.
But Ethernet requires only +1, -1 V
One more thing - I can't found absolute maximum level of voltage on Ethernet pins in TM4C129. So I think It's like on other MCU pins - 3.3 V.
So it's very strange, that all Ethernet ESD protections from TI has DC Breakdown Voltage much more that Ethernet voltage and much more that absolute maximum voltage for MCU pins.
But now I have theree questions.
1. What is the absolute maximum level of voltage on Ethernet pin for TM4C129x?
2. What level of ESD required for Ethernet?
3. Where ESD protection have to be placed - between MCU and transformer or between transformer and 8P8C(RJ-45) connector?