Hi, I am new in this community and got a huge HVAC-project running on Arduino Mega, but now I am running out of speed and space on that board.
I thought of switching over to the TM4C1294 Connected LaunchPad and Energia-IDE.
I have been searching for 2 hours in this forum but I am not quiet sure wether I found the right answer or not.
So please don't mind a Newbie's question:
I want to use the board as a webclient that pulls a code(sketch) from a webserver, stores the .bin or .hex-file in some kind of storage (USB, SD, Flash) on the board and after that resets itself, load the code und will run with it. Is that possible and if is there an example how to do it?
I know that from Mbed, it is working fine but only with the original Mbed-LPCxxx and I don't want to rewrite the whole code to the Mbed-IDE because I am not so familiar with CortexM4 programming.
Would be great to come to Your community, it seems to be a friendly one.
Thank You
Andreas