This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

SDRAM Design Guide: RFSH register setting?

Prodigy 80 points

Replies: 3

Views: 279

Hi,

I'm looking at the Interfacing SDRAM Memory on High Performance Microcontrollers (TIDM-TM4C129XSDRAM) design guide, and I don't understand why the RFSH value is set as it is.

RFSH is set to a value of 1024 at line 435 of the dktm4c129_sdram_performance_example.c file in the provided software example, with a call to EPIConfigDRAMSet():

EPIConfigSDRAMSet(EPI0_BASE, (ui32Freq | EPI_SDRAM_FULL_POWER | EPI_SDRAM_SIZE_512MBIT), 1024);

The system clock frequency is 120 MHz and the EPI clock frequency is set to 60 MHz. The EPI is being used in SDRAM mode.

According to the datasheet for the TM4C129XNCZAD part (sect 11.4.2.2), the refresh value should be calculated as:

RFSH = (t Refresh_us / number_rows) / ext_clock_period

Where:

t Refresh_us = the refresh period for the SDRAM in us.

number_rows = the number of rows in each SDRAM bank (either 4096 or 8192).

ext_clock_period = the period of a single EPI clock period in μs.

The example provided in the datasheet shows how to calculate for a 64 ms refresh period (64000 μs) with a 4096 row part with an external clock speed of 50 MHz (0.02 μs period):

RFSH = (64000 / 4096) / 0.02 = 15.625 μs / 0.02 μs = 781.25

You then pick a value LESS than this to provide some margin.

In the design guide, the SDRAM part referenced is an ISSI 512Mbit SDRAM Memory. The datasheet for this part states that it has "8K refresh cycles every 64 ms." It think that this means that it has a 64 ms refresh period with 8192 rows. With a 60 MHz EPI clock (0.0167 μs period), the calculation becomes:

RFSH = (64000 / 8192) / 0.0167 = 7.8125 μs / 0.0167 = 467.81

How can a value of 1024 be okay in this case? It's much higher that then the calculated RFSH value.


Even if the part actually had only 4096 rows the calculation is:

RFSH = (64000 / 4096) / 0.0167 = 15.625 μs / 0.0167 = 935.63

For which 1024 still wouldn't be acceptable.

Is there something I'm missing or is the example code not correct?

Thanks,

Matt

  • Hello Matt,

    Yes, I accept that the calculation for Refresh count is not correct in the code example and have already submitted a code update request.

    Regards
    Amit

    Regards,

    Amit Ashara

  • In reply to Amit Ashara:

    Alright, thanks for clearing that up!
  • In reply to Matt Chernosky:

    Hello Matt,

    Thanks for checking this and giving us the feedback

    Regards
    Amit

    Regards,

    Amit Ashara

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.