This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Win 10 ICDI Drivers Released

Hello Forum,

The Updated ICDI drivers for Win8 and Win10 has been uploaded to the following link

http://www.ti.com/tool/stellaris_icdi_drivers

The older ICDI drivers is right now pointing to the new package and as the web page transitions it will be corrected in the next 24-48 hrs.

A great thanks to in helping us out with the driver analysis independently

USB drivers for examples of TivaWare will be updated as well with the next release of TivaWare scheduled for Mar-Apr 2016. In the meantime if there any issues with the new ICDI drivers or older USB example drivers, please respond to this post.

Regards

Amit

Regards,

Amit Ashara

16 Replies

  • The download link appears to be broken.  Clicking it just opens the png using either Edge or Chrome.

  • In reply to Dan Beadle:

    Hello Dan,

    Replaced it with the URL. Seems to be an editor issue

    Thanks Regards
    Amit

    Regards,

    Amit Ashara

  • In reply to Amit Ashara:

    I still just get a png link.
  • In reply to Dan Beadle:

    OK, I see that you put the link just above the graphic in the first post:

    http://www.ti.com/tool/stellaris_icdi_drivers

    The buttons still are just graphics.  I was able to enter the address and get the driver.

    Thanks

  • In reply to Dan Beadle:

    Hello Dan,

    OK Now I get it. The Image is of how the page will appear when the user clicks on the link. Let us know if the new drivers worked.

    Regards
    Amit

    Regards,

    Amit Ashara

  • In reply to Amit Ashara:

    , please tell me that the drivers are signed now. I had just last week a call from my old high school professor trying to install the drivers, which he couldn't


    Luís Afonso

    For more reply options press "Use rich formatting" on the bottom right.

    I have a blog that i am making to help some colleagues with learning Tiva:  https://sites.google.com/site/luiselectronicprojects/home
    I have here now example codes for the Tiva more organized: https://github.com/LuisAfonso95

  • In reply to Luis Afonso:

    Hello Luis,

    Double click on the .cat file. If it shows the image as below then they are signed correctly. We have tested it on a Win10 VM and they work correctly.

    Regards

    Amit

    Regards,

    Amit Ashara

  • In reply to Amit Ashara:

    Yay, no more "turn off enforced signed drivers" process.


    Luís Afonso

    For more reply options press "Use rich formatting" on the bottom right.

    I have a blog that i am making to help some colleagues with learning Tiva:  https://sites.google.com/site/luiselectronicprojects/home
    I have here now example codes for the Tiva more organized: https://github.com/LuisAfonso95

  • In reply to Luis Afonso:

    Hello Luis,

    The real test is out in the field. In house testing can only be a process check.... Real issues come from the field.

    Regards
    Amit

    Regards,

    Amit Ashara

  • In reply to Amit Ashara:

    Hello,

    I'm running the TivaWare C-series usb_dev_cserial example for the ek-tm4c1294xl board and I'm still not able to get Windows 10 to recognize the board as a USB COM device. Under device manager the USB device is listed the same as under Windows 8, TivaWare USB serial port but any time I try to connect to it I get an error. I tried the update in this thread assuming the stellaris update would work for TivaWare but no luck. I also did have to disable driver enforcement even though it looked like the .cat file showed the correct signature.

    The same exact board connected to a Windows 8 system works fine. Anything I can do to help resolve this issue so that the board works on Windows 10?

    Thanks,
    Juan

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.