The project I'm on is a resurrection of a project from a different company. I've pieced together the tool chain and am at the last stages (I hope). I'm trying to create a bin file but have not been successful.
I have succeeded with creation of an out file (no compilation or link errors).
I am using the TI supplied batch file (tiobj2bin.bat) without modification.
I am in Brut force mode... My command is:
"C:\ti2\ccsv5\utils\tiobj2bin\tiobj2bin.bat" ".\SAMPLEit.out" ".\SAMPLEit.bin" "C:\ti2\ccsv5\tools\compiler\arm_5.1.1\bin\armofd.exe" "C:\ti2\ccsv5\tools\compiler\arm_5.1.1\bin\armhex.exe" "C:\ti2\ccsv5\utils\tiobj2bin\mkhex4bin.exe"
The output has numerous outputs of:
Load address not computed for file that does not have a segment table at XML_TI_OFD.pm line 1433
Use of uninitialized value in multiplication (*) at script/mkhex4bin.pl line 285.
The output also has numerous outputs of:
warning: section .\SAMPLEit.out(.text) at 027662h fall in unconfigured memory
(skipped)
How do I fix these issues?
Any help would be greatly appreciated.
Kim