Part Number: RF430CL330H
First I have to point out that I have no experience in RF design, so I might as trivial questions here.
I am trying to include an NFC tag and antenna using the RF430CL330H on a device.
I calculated the inductance of the antenna coil when designing the PCB to be slightly under the recommended 3.85uH. It's only after that I realized I should have aimed at a lower value in the PCB and tune it with the capacitor.
Anyway, after assembling the PCB (I put the footprints for tuning capacitor, but I left them empty), I got the attached measurement screenshot using a MiniVNA and a loop antenna placed above my tag (all components in place, no power applied to the tag).
As I understand, I need to increase the tuning capacitor to adjust the frequency down from 14Mhz to 13.55Mhz. But I measured some tags, and they are at 14Mhz, so there must be something wrong with my design. (my antenna is 40mmX40mm 8 turns).
First screenshot is with all components in place, second screenshot is antenna with no components.
My questions:
- On the graph, the blue line has a really weird shape. I am not sure I get what the RP° represents. As I understand it has something to do with Q factor, but not sure what this is either.
- I measured my design using a loop antenna because I didn't think of putting test connector on my board. Is the loop antenna technique enough, or should I make a new board with a test sma connector on it?
- I read a lot of documents from NXP, ST and TI about antenna design, but they mostly focus on designing antenna for the readers, not for the tags. I read your SLOA197 too, but I still think I am missing something.