Other Parts Discussed in Thread: TPS2052B
Good morning everyone.
I have a few questions to ask. I have been using the EK-TM4C1294XL to try some code to see how it performs using the ICDI Debugging port connected to my computer. Now i need to mount it to a prototype and power the microcontroller with a battery. To accomplish that, i've bought a LM7805 regulator using the fixed-output scheme to power it from a battery of 12V by the BoosterPack interface.
My first concern is that I can't find in the schematic the BoosterPack pin that i should connect the regulator's output to. The JP1 scheme (Power Control Jumper) doesn't show if the pin n°1 is mapped to another pin of the BoosterPack interface.
Also, should i care about TPS2052B not providing current limit protection using the LM7805? Must I also connect an specific GND to the regulator's GND ?
Finally, can I compile and run a program using the ICDI-Debug USB while powering the microcontroller with the BoosterPack interface?
I hope you have not been overwhelmed with my questions.
I apologize for my bad english. it's not my native language.
I hope somebody can help me out.
Best wishes,
José