Part Number: DK-TM4C129X
Hi there,
I'm using the TM4C129X dev board with grlib demo project and Tivaware version SW-TM4C-GRL-UG-2.1.4.178.
I added an Extended font to the project via the "ftrasterize" tool and it works well with the basic Latin alphabet characters.
When i tested the Western European accented characters I saw incorrect characters rendered! For example "ã©" instead of "é".
I suspected the tool generated font, so I have used the Extended Font included in Tivaware (g_sFontExHandwriting22) but I got the same issue.
I changed the source text codepage via GrStringCodepageSet(...) to CODEPAGE_ISO8859_1 and CODEPAGE_UTF_8 and I have always the same issue.
Can someone help me please?