Hello
We are working on Tiva MCU TM4C1294NCZAD, using Tivaware 2.1.4.178, trying implementing MSC class on USB with an external NAND Flash. We started from usb_dev_msc example, which uses mx66l51235f EEPROM.
Currently our PC sees it an external device when connected (but doesn't recognizes it as formatted even if a file system in installed on board), but after a while it disappears.
Sectore size of our Nand Flash (whose driver is working for write and read operations) is 2048 Byte, while is 4096 Byte in the EEPROM used in the original example. Is it possibile to use the USB library with this sector size? How should we adapt USB library or usb_dev_msc file to work with this size?
Thank you