Other Parts Discussed in Thread: EK-TM4C1294XL
I am unable to connect my crypto connected launchpad with the exosite cloud server. I have already programmed with the secure IOT demo.
The board MAC Id is given properly and its not connected any other users.
Able to add the board but unable to activate it even after the board is connected to the FTTH connection without any login requirement.
This device has not yet been activated or does not exist. Please activate your device or confirm the device RID and try again. (in the exosite account)
MAC Address: 0800285a9035
Network Added: If-1:192.168.1.13
Service Status: DHCPC : Enabled : Running : 017
Resolving IP address of time.nist.gov...
NTP IP resolved to 132.163.97.2
Connecting to NTP server
Current Date/Time is Thu Dec 13 09:28:51 2018
CloudTask: Failed to create a new TLS instance. Exiting.
After running in CCS