This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CCS/TM4C1294NCPDT: Fix "through" in bootloader comment

Prodigy 90 points

Replies: 1

Views: 102

Part Number: TM4C1294NCPDT

Tool/software: Code Composer Studio

In "tivaware_c_series_2_1_4_178" there is text:

"where ENET_MAC_ADDR0 though ENET_MAC_ADDR2"

that could be corrected (by adding "r": "though" -> "through") to:

"where ENET_MAC_ADDR0 through ENET_MAC_ADDR2"

in line 874 of files:

examples/boards/dk-tm4c123g/boot_serial/bl_config.h
examples/boards/dk-tm4c123g/boot_usb/bl_config.h
examples/boards/dk-tm4c129x/boot_emac_flash/bl_config.h
examples/boards/ek-lm4f232/boot_serial/bl_config.h
examples/boards/ek-lm4f232/boot_usb/bl_config.h
examples/boards/ek-tm4c1294xl/boot_emac_flash/bl_config.h
examples/boards/ek-tm4c1294xl/boot_serial/bl_config.h
examples/boards/ek-tm4c129exl/boot_serial/bl_config.h

Best wishes,

Piotr Kasprzyk

  • Thank you for catching this. I have entered this correction to our issue tracking system so that it may be corrected for the next release.

    Best Regards,
    Bob Crosby

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.