Other Parts Discussed in Thread: EK-TM4C1294XL, UNIFLASH, CC3100SDK, CC3120, CC3100, MSP-EXP432E401Y, CC3120BOOST, CC31XXEMUBOOST
Tool/software: TI-RTOS
Hello,
I just received 2 test kits:
EK-TM4C129EXL and C3120BOOST.
Im trying to test the TIDM-TM4C129XWIFI example but I'm not able. I know this example is for the EK-TM4C1294XL and not exactly for my launchpad but from what I have checked, the boards and the processors for that application are "identical".
I can compile the project (several warnings in the compilation) and program the EK-TM4C129EXL. But it gets stuck in the void function HttpSetup () on the LOOP_FOREVER () line; located in main.c. Follow the attached project.
Regarding the C3120BOOST I can't program it. I'm connecting it to BoosterPack1 in the launchpad. Is there any change that should be made to the card or can I not program it through this card? Follow the attached error print.
Here are the versions of the software I'm using:
CCS: 8.3.0.00009
UNIFLASH: 4.6.0
TI-RTOS: 2.4.0.10 (INCLUDED TivaWare_C_Series-2.1.1.71b)
CC3100SDK_1.3.0
XDCtools: 3.31.1.33