Tool/software: Linux
I am using CCS V9 and reading the SPRUHU5D. At 8 of 3.1, it says that Use the Step 3 link to change the connection used to communicate with the board. The current setting is shown in the Resource Explorer page for the selected example. (If you want to use a simulator instead of a hardware connection, double-click the *.ccxml file in the targetConfigs folder of the project to open the Target Configuration File editor. Change the Connection as needed, and click Save.).
Where can I find the "Debugger Configuration" as shown in the picture for Step 3. I did try from Run->Debug Configurations menu, but there is nothing like Debugger Configuration icon and did not find "targetConfigs folder of the project" also.
Can anyone help this? Thanks
Neil