Tool/software: TI C/C++ Compiler
How to save 2D array values into TM4C1294 EEProm,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
How to save 2D array values into TM4C1294 EEProm,
I am not sure if I understand your question. A 2 dimensional array is stored in RAM as a single buffer. You can use the EEPROMProgram() function to program that buffer into the EEPROM. Here is a very simple example programming a 2 dimensional array into EEPROM and then reading it back into another 2 dimensional array.
#include <stdint.h> #include <stdbool.h> #include "inc/hw_types.h" #include "inc/hw_memmap.h" #include "driverlib/sysctl.h" #include "driverlib/eeprom.h" //***************************************************************************** // // Main 'C' Language entry point. // //***************************************************************************** uint32_t array[4][6]; uint32_t array2[4][6]; int main(void) { uint32_t ui32SysClock; uint32_t i, j; // // Run from the PLL at 120 MHz. // ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ | SYSCTL_OSC_MAIN | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000); // Initialize the EEPROM SysCtlPeripheralEnable(SYSCTL_PERIPH_EEPROM0); EEPROMInit(); // initialize the array for(i = 0; i < 4; i++) { for(j = 0; j < 6; j++) { array[i][j] = i * j; } } // program array into EEPROM starting at first EEPROM address EEPROMProgram((uint32_t *)array, 0U, sizeof(array)); // Now read from the EEPROM into the second array EEPROMRead((uint32_t *)array2, 0U, sizeof(array2)); }