Hello,
I´m using ADC 0 with sample sequencer 0 (6 channels) and ADC 1 with sample sequencer 2 (4 channels). To transfer the data I´m using the DMA with ping pong mode. I re-enable the transfer channels in the corresponding interrupt handler. Now my problem is that the order of the adc channel in the destination buffer of the dma is not the same as in the sample sequencer because it´s changing always.
Example:
Sample Sequencer -> DMA Destination Buffer
1. CH1 CH2
2. CH2 CH3
3. Ch3 CH1
Is there any trick to get the same order in the destination buffer as in the sample sequencer? Because if I wanna process the data I have to know which place in the destination buffer is which channel.