Hello,
Can FlashProtectSet() in the flash region that is protected as Execute-only works fine?
After protecting the flash region A as Execute-only by setting FlashProtectSet(), I tried to execute FlashProtectSet() on the flash region A for next flash region B .
But then, fault ISR is called.
I configured linker command file and set --embedded_constants to off with reference to below thread, but the problem is remained.
If the answer for my question is no, are there any way to execute FlashProtectSet() on the execute-only flash region?
Regards,
U-SK