Other Parts Discussed in Thread: ISO7521
Hi Team,
We are interfacing a Tiva(TM4C1294KCPDTI3) processor with C2000 via ISO7521. We are observing a dwarf pulse that is only around 960mV tall on the UART line. The tiva is powered from an isolated winding of the flyback while the C2000 is powered by another isolated winding. There is Y-cap (2.2nF) that links the positive DC bus voltage on the flyback primary winding to iso GND of the TIVA powered isolated winding. With just the Y cap they observe the 960mV pulse but when they add damping resistors (2x 100Ohm) in series with that Y-capacitor the pulse is transmitted properly at 3.3V. When observing the UART lines with and without the resistors there is a clear difference in the amount of added noise. The low voltage pulse is an issue because it is not transmitted by the digital isolator and causes data loss.
We suspect the Y cap is providing a feedback path that is adding noise to the Tiva lines. The resistors potentially dampen this noise which is why the issue is removed when they are added. We are trying to understand why the presence of noise causes the device to act in this manner. Have you ever observed an issue with a Tiva UART line outputting pulses of lesser magnitude? If so, could this be caused by noise and why does this manifest as lower magnitude pulses? Thank you for any guidance you can share.
Regards,
Garret