Hello Sir,
In this forum they have told that USB-Host is working.
So, can you please share the code for USB-Host for RM48 controllers.
Best Regards,
Praveena M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Sir,
In this forum they have told that USB-Host is working.
So, can you please share the code for USB-Host for RM48 controllers.
Best Regards,
Praveena M
Hi Praveena,
I don't have USB host example code. I tested USB code from Micrium before, and you can download the code from Micrium webpage.
The uCOS is also released on github under apache (free), it includes the host driver.
Hello Wang,
Thank you for your reply.
I had downloaded the code from micrium.
But the problem is micrium developed the code in IAR-IDE.
I need the code in CCS-IDE.
Can I import IAR code to CCS?-----------> If yes, please tell the procedure.
Best Regards,
Praveena M
Hi Wang,
Do you have any idea on IAR-IDE.
I am able to open the project.
Now, if I download and debug and then run, it is not printing anything on Terminal I/O.
So, can you please help me how to print in Hyper terminal / Terminal I/O, as early as possible.
Best Regards,
Praveena M
Hi Wang,
Here, you have told that you tested the code.
Can you please tell me in which IDE you had tested the code and how it is tested.
Thanks & Regards,
Praveena M
Hi Praveena,
Micrium used CCS IDE during code development, and I helped them test the stack (USB,and TCP/IP).