Other Parts Discussed in Thread: HALCOGEN
Dear Sir/Madam,
I am using the TMS570LC4357 Hercules safety MCU development kit. I am having trouble with using many of the N2HET2 bits as GIO outputs on their default terminals. An example here is N2HET2[09], the default ball is L16 and the alternate ball location is K17. When I mux N2HET2[09] to K17 I am able to drive it as an output without any issues, however when I try to use it unmuxed I am unable to drive output on default terminal L16 with otherwise the same settings.
The datasheet is a little confusing on whether it is even possible to use L16 as an output. Ball L16 is not in the output mux table (6-1 in the datasheet) but I had interpreted this to mean that while this was not a muxed ouput pin, it could still be used as an output.
Could you confirm whether or not it is indeed possible to use L16 as an output? If it is possible what could I be missing in Halcogen? Or could this be related to the Hercules development kit? Is it the same for many of the other pins in N2HET2?
Kind regards,
S Grimm