Hello
I am looking to add new features to a couple of our products which use the TM4C129ENCPDT but am starting to reach limits of flash and RAM.
Before I look to other processors such as STM32 I was wondering what is happening with the TM4C129 family.
We use the TIRTOS which has had no updates since 2016 and the chip itself has had no new variants added and seems to be pretty set at what we currently have.
With the extra memory required to add things like TLS and VOIP we are looking to other devices which provide the compactness of a single device with the nice features such as USB, Ethernet, SPI, I2C but with more memory. I know we can add extra external memory, but that defeats the purpose of using a single chip micro.
I saw another post which says TM4C129 is still actively supported and TIVAWARE has been updated, but the TIRTOS and NDK are sitting idle and we already are using LWIP in some of our TIVA devices because the stack has more features and active maintenance.
Can someone tell me if TM4C129ENCPDT is worth holding onto, or should we be looking at alternatives going forward.