Hi.
We use ADC1[9] and ADC1[31].
If only ADC1[31] is converted, the conversion result will be about 50. And if you convert only ADC1[9], the conversion result will be 4095.
But If you convert two(ADC1[9] and ADC1[31]) at the same time, the conversion result will be 4095 for both.
I expected both conversions to be 4095, but that's not the case. Why is the conversion result different when only the ADC1[31] is converted?
Best regards.