This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS0714: TMS570LS07 problem in erase data from eeprom using fee driver erase function

Part Number: TMS570LS0714

hi 

I am using fee driver with  TMS570LS07  and I realy need help to know how i can erse all the block or the adress i want in eeprom 

I tried the code below but it does not work so please can any one help me 

my code is here 

#include "ti_fee.h"

#include "sys_common.h"
#include "system.h"

uint16 u16JobResult,Status;
Std_ReturnType oResult=E_OK;
unsigned char read_data[100]={0};

uint8 SpecialRamBlock[100]={30,31,32,33};

unsigned char pattern;
uint16 u16writecounter;

unsigned int  FeeVirtualSectorNumber;
unsigned char VsState, u8EEPIndex;
unsigned char u8VirtualSector;
uint8 Test_Recovery;
uint8 Test_Cancel;

uint8 *adress_of_block;
void delay(void)
{
    unsigned int dummycnt=0x0000FFU;
    do
    {
        dummycnt--;
    }
    while(dummycnt>0);
}

void main(void)
{
/* USER CODE BEGIN (3) */
    unsigned int BlockNumber;
    unsigned int BlockOffset, Length;
    unsigned char *Read_Ptr=read_data;

    unsigned int loop;

    /* Initialize RAM array.*/
    //for(loop=0;loop<100;loop++)SpecialRamBlock[loop] = loop;

    /* Initialize FEE. This will create Virtual sectors, initialize global variables etc.*/
    TI_Fee_Init();
    do
    {
        TI_Fee_MainFunction();
        delay();
        Status=TI_Fee_GetStatus(0);
    }
    while(Status!= IDLE);

    TI_Fee_EraseImmediateBlock((uint16_t)0xF02001D8);
    do
    {
        TI_Fee_MainFunction();
        delay();
        Status=TI_Fee_GetStatus(0);
    }
    while(Status!=IDLE);
    /* Write the block into EEP Asynchronously. Block size is configured in ti_fee_cfg.c file. Default Block size is
       8 bytes */
    BlockNumber=0x1;
    TI_Fee_WriteAsync(BlockNumber, &SpecialRamBlock[0]);
    do
    {
        TI_Fee_MainFunction();
        delay();
        Status=TI_Fee_GetStatus(0);
    }
    while(Status!=IDLE);


//    //here block number is our start block to write then our buffer will fill the blocks which after him untill
//    //our buffer write all its data
   BlockNumber=0x1;
    /* Write the block into EEP Synchronously. Write will not happen since data is same. */
//    TI_Fee_WriteSync(BlockNumber, &SpecialRamBlock[0]);

      BlockOffset = 2;
      Length = 0xFFFF;
      oResult=TI_Fee_Read(0x1,BlockOffset,Read_Ptr,Length);
      do
      {
          TI_Fee_MainFunction();
          delay();
          Status=TI_Fee_GetStatus(0);
      }
     while(Status!=IDLE);

    /* Invalidate a written block  */
//    TI_Fee_InvalidateBlock(BlockNumber);
//    do
//    {
//        TI_Fee_MainFunction();
//        delay();
//        Status=TI_Fee_GetStatus(0);
//    }
//    while(Status!=IDLE);

    /* Format bank 7 */
    //TI_Fee_Format(0xA5A5A5A5U);

    while(1);
/* USER CODE END */
}

i tried to delete all of that data but i could not i just need to know how to erase full memory or data of an address