The contents read through USB DFU begin with an 8 byte record, supposed to be the programming commands for possible downloads. The record content is: 01 00 06 00 00 e8 03 00, which specifies that the flash will be programmed from block number 6! I'm quite confused here, should it be block number 0? Another issue is that I have two "broken" EK-TM4C123GXL, which will not enumerate as nothing if plugged to a USB host by the ICDI USB port. But it seems that it is still working as the led blue-red-yellow is blinking as usual. Is ICDI in some locked up state in this case?