Tool/software: TI-RTOS
Hello,
I am developing an application in TM4C1294NCPDT processor and using TI-RTOS 2_16_01_14 with NDK 2_25_00_09. I have already implemented my network connection using the Ethernet interface and it is working fine. Now I have a GPRS Modem connected to an UART port and I am communicating with it using AT commands. The Modem has an internal TCP/IP stack but of course I need to use AT commands to connect, disconnect and control the connection. Iwould like to use the same code (I mean, sockets) I have written to communicate over GPRS (In that case, UART). I have noticed that I need to use PPP interface available in NDK but I don't know how to put it to work together with my UART.
What I need is, once I am attached and connected to the GPRS network, I want to open a socket with my server and send/receive packets, transparently, even I am using ethernet or gprs.
Any advice?
Tks in advance