Tool/software: TI-RTOS
Hi,
I have created two Hwi ISR using .cfg file with default priority set i.e. -1 for GPIO(interrupt number 23) and SPI-DMA(interrupt number 46) and also i have created two timer ISR(timer 1 and Timer 3) using cfg file. Both timers are up counter and running periodically. dont have any option to set the timer priority in cfg file.
Now i want to understand how to set the priority for the timer ISR? I need reduce the priority of timer ISR than the HW ISR if its having higher priority than the HWI ISR. i dont have any issue if both timer and HWI ISR running with the same priority.
Regards
Bala