I've struck a couple of problems using GUI Composer v2 standalone App.
I have a board based on the EK-TM4C123GXL and a simple GUI composer App with a couple of labels and a button. The target blinks a LED and increments a counter. The counter is displayed in the GUI (as a label widget) and can be seen to be incrementing. After a couple of minutes, the counter in the GUI stops and the LED on the target has stopped.
Clicking the Disconnect button in the GUI starts the LED blinking again. Connecting the GUI again the counter can be seen to have advanced, it matches the number of times the LED blinked.
This is on a small older Windows 10 laptop, with gcruntime6.0.0 and GUI Composer v2 standalone App exported from the online tool. I've tried another Windows 7 laptop and had the same issue. A newer Windows 10 laptop ran for longer but still freezes up occasionally. A (this year) new Windows 10 i7 Desktop will run for hours no problem.
Is there a minimum spec for GC on a PC?
The other problem I struck is when the laptop is out of Wi-fi range the Standalone App will not connect to the target - in the status bar it reads "Connected to TI Cloud Agent.ccxml string contains %SERIALPORT% - must resolve before calling". After bringing the laptop back into Wi-fi range it still does not connect and I end up restarting the App to attempt to connect again.
thanks