we use arm load fpga.bin from flash , arm send the fpga.bin to the fpga to initiate fpga.
there is one FPGA(7A200T), one ARM(tm4c1294),one FLASH(N25Q)in our board.
1. arm connect with flash, fpga connect with arm;
2. fpga configration mode[111], slave serial;
3. power on, arm set program_b high, then low, set high again , arm read the init_b, the value is high.
4. arm read fpga.bin from the flash, and send the packet to the fpga use spi, the packet is 1024byte each time, the fpga.bin is 7MB;
5. arm finish the send packet, find the done signal is low always.
which step is error? give me some suggestion,thanks.