Hello,
My customer is running into two issues when they try to evaluate the EVM:
1) When I run a DC motor in PWM Mode at 12V, 100% PWM @ IN1, and no output load my Power Supply is reporting roughly 0.550A to run the motor and the eval PCBA. When I measure the voltage on the IPROP1 pin, I am seeing about 0.190V across the 390 ohm resistor, which translates to 487.2 uA. With the gain of 1100 A/A, this is 0.536A of motor current. At this same time, the GUI is reporting 0.937A:
The GUI is configured for the 390 ohm resistors. Is there something I am missing that is causing such an error to be reported on this screen? It also seems to “latch” at a specific value, is there a sampling/refresh rate that the GUI updates these values at as well as the resolution on the ADC used here?
2) When I have Open Load Detection Enabled, every time I start the Motor the nFAULT red LED is turned on (and can be cleared when toggle the Sleep input via the Wake Slider). When I disable the Open Load detection the nFAULT is never tripped. I am confused as to how this is happening. If it is the Open Load Detection that is tripping the nFAULT, it looks like it is only checked in the HW version on start-up or coming out of sleep mode per the datasheet and the error is still occuring otherwise.
Any help is greatly appreciated!
John