Hi .
As the title ,my application the BLDC can't start-up success at sometimes.
I got the print information of DRV10987. Regster 0X00 Value:0004( lock2 ,abnoamal Kt),Kt value=12.38, Speed=2580 RPM(the FG frequence is 172Hz,my closed threshold is 179.2Hz).
Abornally ,the BLDC doesn't enter closed loop state.My config Kt=10.12 and the setting range of KT is between 2kt and 1 / 2kt.The Kt=12.38 is in the normal range
I don't understand why the error of KT is reported at this time.
When lock2 is triggered,then the U/V/W will set Hi-Z and reset the register,about 5s(t lock-off) after restart the BLDC? but my applycation is that when lock2 is triggered,
about 3s after the kt=6.88, Spd=9250(FG frequence is 595Hz),seems have entered the closed loop .
Please help to see how to solve this problem ,ths.
Following is my EEPROM config:
90:0X102E
91:0X0B3A
92:0X08C0
93:0X12EB
94:0X3F0F
95:0XF843
96:0X006A
Motor parameters :
Best wishes and regards!
chris