This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8711: Pre-driver fault occurs everytime with CSD88539ND

Part Number: DRV8711
Other Parts Discussed in Thread: CSD88539ND, CSD88537ND

I use DRV8711 with IRF7351in custom board (motor current up to 5A, supply voltage up to 48V). Then i try change mosfet to CSD88539ND in same board, but now I am constantly getting Predriver Fault when the supply voltage is greater than 30V. 

No recommendations from this forum have yielded results. The transistors are very similar in characteristics. Which of their parameters can affect this error?