・tOL Open load detection time MAX200ms
・IOL Open load current threshold TYP30mA
What percentage of tolerance threshold is guaranteed for each value?
If the guaranteed value is an absolute value, please let us know as well.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
・tOL Open load detection time MAX200ms
・IOL Open load current threshold TYP30mA
What percentage of tolerance threshold is guaranteed for each value?
If the guaranteed value is an absolute value, please let us know as well.
Teauka,
・tOL Open load detection time MAX200ms
200mA is an absolute maximum value.
・IOL Open load current threshold TYP30mA
30mA is typical open load detection current. According to 6 sigma data, the minimum value is 21mA; the maximum value is 38mA over full temperature range.
Regards,
Wang
tOL Open load detection time MAX200ms
Is there any 6σ deviation data for the above?
Teauka-san,
The standard deviation is about 4ms with 13.5V and 48V input. The mean value is about 150ms.
Regards,
Wang Li