Hi team,
I have questions to DRV3205-Q1.
Can the gate resistor of MOSFET be removed? Or, should gate resistor use for DRV3205-Q1?
Regards,
Nishimura
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I have questions to DRV3205-Q1.
Can the gate resistor of MOSFET be removed? Or, should gate resistor use for DRV3205-Q1?
Regards,
Nishimura
Nishimura-San,
This depends heavily on the FET used, the gate drive current, the PWM switching frequency, and the output VDS rise and fall time needed.
If the customer can give us this info then we can help decide if gate resistance is needed.
Regards,
-Adam
Hi Adam,
Thank you for your answer. Customer wants to check the Rgate necessity by design point of view.
Customer will evaluate the DRV3205-Q1 without Rgate on their application. In this case, if customer checks the DRV3205-Q1 doesn't need Rgate and it seems there is no issue, customer can use DRV3205-Q1 without Rgate? Or, for design reason of DRV3205-Q1, is it needs to use Rgate?
Regards,
Nishimura
Nishimura-San,
If the customer is using more than one FET per gate output, then gate resistors are needed. This app note discusses the same topic for another similar driver: https://www.ti.com/lit/an/slvaf39a/slvaf39a.pdf?ts=1623094793659&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FDRV3255-Q1%253FkeyMatch%253DDRV3255%2526tisearch%253Dsearch-everything
If the customer is using only one FET per gate and the IDRIVE setting selected does not cause overshoot/undershoot/ringing on the gate or source lines then they do not need a gate resistor.
Regards,
-Adam
Hi Nishimura-san,
Do you need any further help on this thread?
Thanks,
Matt