Part Number: DRV8432
Is there has the data of Static power consumption of DRV8432, PVDD=25V and 50V, in PBTL、BTL、SE mode. For there is only static power consumption of GVDD in datasheet.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ryan,
My customer Harman use this power stage as a lass-D audio amp, so we concern that if there is no music signal input, but also a 50% duty PWM input, in this condition, how much is the total power consumption ?
Yang,
Again, if there is no current in the load, then there will be no current from PVDD. PVDD only supplies the high-side internal FETs. It is completely dependent on the load conditions. If no voltage drop across the load, it should be nearly zero.
Regards,
Ryan