This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8847: DRV8847PWR: Unsure why it wont run nema

Part Number: DRV8847

I am trying out the drv8847pwr as my prototype as nema 17 stepper motor driver. I have tried 2 stepper motor on the breadboard with similar configuration and only swapping out stepper motors. Below is my setup:
Stepper motor A: www.ebay.com.au/.../173343080042
Stepper motor B(48steps): www.digikey.com.au/.../417812

My setup is "4 capacitors 470uf" and a 10uf capacitor setup near to the VM, Both isense is gnd, the mode is not connected. Sleep pin is logical 3.3v high. Trq are not connected. Both ISENs is tie to ground for now.
Don't think heat is a problem, but I have placed the heatsink on top of the drv8847.
I have I have no issues running clockwise fullstep the `stepper motor B` where the VM is 5V.

However, `Stepper motor A` with higher current 0.7A per phase is not moving at all at VM at 3.0V. Any idea what went wrong with my setup?