Hi,
The Drv8353H is a 100V mosfet driver chip, I use it in my servo drive system which drive a 36V motor, or a 48V motor, and even a 60V servo motor. It seems to work normally. My question here is, the chip can be used in a 72V servo motor drive system ?
Thank you.