This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Driver to control a 110V/220V 600W AC Motor Speed

Other Parts Discussed in Thread: UCC27712

Hi, 
I have to control the speed of an AC motor and I need some reference design and guidelines to design my own speed controller for an AC motor. Right now, I have a 110V AC motor but it would be better if I can design a universal driver for 100V to 240AC Motors. Any help or suggestion is highly appreciated. 
I attached a link to the AC motor that I have right now. Thanks

https://ml-motor.en.made-in-china.com/product/WKcnkZFocdVB/China-China-Manufactury-Strong-Suction-Small-Motor-Home-Used-for-Vacuum-Cleaner-ML-H3-.html