Hi, Team,
My customer found the offline diagnostic time for the OLSC should be so long. Customer enable the OLSC by EN_OLSC, then setting the PD_SHx and PU_SHx in 10ms. They found the SHx pin should take >1 second to change to 1/2 VDD, which should be the right status for the DRV8718. And customer need to wait >1s to get the right diagnostic result.
Is it the normal working process for the DRV8718? Can we reduce the diagnostic time for DRV8718?
Following is the waveform, and the green one is the SHx's output.