Using ERM motors, open loop with software command. I am writing to register 0x04 on the fly in code. Can I do this without going to standby? Seems part hangs up and won't respond.....Is there some sequence that must be done?
Also if motor is to operate at a given period (say 1 sec) do I have to wake up and send a GO command each time or is there a period register in the device I can write to which will automatically pulse the motor?
Thanks