Other Parts Discussed in Thread: DRV8833
Hi Team,
My customer now use DRV8833C in printer solution (phase register is 10 ohm and current is 300mA)
① Customer now both AISEN and BISEN are connected to GND. How big is the Ichop current instantly? Is it 5V/10Ω=500mA? Or bigger? Can 8833C bear it?
② If the instantaneous current is very large, do customer need to connect a 1~2Ω resistor to AOUT1 or AOUT2 to increase the current limit when designing?