Other Parts Discussed in Thread: DRV8899-Q1
I'm currently working to control a stepper motor using the DRV8899-Q1EVM board with SPI commands. The current behavior is that the board will either respond with an incorrect word format on the Status bits or will not reflect the data being written on the Report bits. After several write attempts the Fault LED turns on.
I can see that I'm sending the correct SPI word with the oscilloscope and my sniffer tool, so I'm really not sure if I'm missing something.