EN_SR_BLANK bits are recommended to be set to "1" when controlled in Smart tune Dynamic Decay mode.
How do I use it? Also, please tell me why.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
EN_SR_BLANK bits are recommended to be set to "1" when controlled in Smart tune Dynamic Decay mode.
How do I use it? Also, please tell me why.
Teauka-san,
Set "EN_SR_BLANK" =1 when controlled with slow-slow or either smart tune decay modes.
Either smart tune decay could have slow-decay operating. Additional blanking time is beneficial in case the stepper motor has excessive parasitic coil capacitance. Also, the blanking time can avoid the switching noise on the current sensing circuit during the power FET turn-on.
For example: when SLEW_RATE [1:0]=00b, the slew rate is 10v/us. With the highest input voltage 45V, the turn-on time is about 4.5us. 5.6us blanking time can avoid the switching noise in to the current sensing circuit.
Regards,
Wang Li