Hello Team,
We would like to interface MAXON EC90 Flat Motor (Brushless DC Geared Motor) with DRV8353RS EVM. We are using Texas MCU which came default with this EVM (ISO-F2807F). We used DRV8353RS GUI to run the Motor, and the Motor is not rotating. With reference to this datasheet ( InstaSPIN-FOC and InstaSPIN-MOTION User's Guide (Rev. H), We found that only BLDC motors with no load can work well. So, Are there any possibilities available for this MAXON EC 90 Motor? We also tried updating the user.h files as per motor specifications. Yet the same issue occurs.
Thanks and Regards
JESINTHA E