Other Parts Discussed in Thread: LAUNCHXL-F28069M, , DRV8305, DRV8312, DRV8301, MOTORWARE, BOOSTXL-DRV8323RH, DRV8323, BOOSTXL-DRV8301, CONTROLSUITE
Hi,
I have Launchxl-F28069M and BOOSTXL-DRV8323RS to control BLDC. I download BOOSTXL-DRV8323RS labs and build. But the project only InstaSPIN-FOC. I want to use InstaSPIN-Motion but it don't have any project.
1. Does BOOSTXL-DRV8323RS have any InstaSPIN-Motion project to download?
2. Should I modify InstaSPIN-Motion project to generate a new case so that BOOSTXL-DRV8323RS can be used? I see some board pin map and circuit diagram are not as same as BOOSTXL-DRV8323RS.
3. If I edit project, is there a risk of damaging the circuit board?
4. From which board should I start to edit the file?(Drv8301,Drv8305,Drv8312)
I mainly use QEP as the basis for speed control. QEP is not used in instaSPIN-FOC.
And instaSPIN-Motion provides QEP speed control, so I want to use instaSPIN-Motion to control the motor.
Can you give me better advice?
Thanks